主题中讨论的其他部件: DS90UB927Q-Q1
我的问题是,我们是否有2台设备作为视频链接至1个显示屏触摸组合模块,如下所示
当I2C被触摸控制器占用到MPU时,我们如何控制DS90UB948-Q1的任一链路?
是否可以使用GPIO:开路低电平/有源高电平以控制DS90UB948-Q1?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的问题是,我们是否有2台设备作为视频链接至1个显示屏触摸组合模块,如下所示
当I2C被触摸控制器占用到MPU时,我们如何控制DS90UB948-Q1的任一链路?
是否可以使用GPIO:开路低电平/有源高电平以控制DS90UB948-Q1?
您好Steven
感谢您的回复。 我只想确保"设备功能模式中的2通道FPD -链接III输入/单链路OpenLDI输出为
为OpenLDI输出从2个输入中选择一个/为OpenLDI输出合并2个输入。 这是很好的不同。 前者意味着2条输入数据路径作为管道进入单个输出,后者意味着" 2条输入数据路径仅允许任一路径为输出"。 根据您对方框图的回答,我们现在可以肯定地将DS90UB948-Q1用作2台DS90UB927Q-Q1基础设备中任一台设备的交换机。
这是我关于DS90UB948-第1季度的最后一个问题。 在数据表第6 - 7页中,如以下屏幕截图所示:
GPIO5 ~ GPIO8_REG GPIO的寄存器只读/写GPIO引脚的用途是什么? 它们与MODE_SEL PIN有何不同?
为了我了解MODE_SEL引脚用于如下所示的设备功能模式选择。 我对吗?
如果我想控制DS90UB98-Q1,我应该使用GPIO5_REG ~ GPIO8_REG权限? 因为只有指定的GPIO才能够进行读/写寄存器?
什么是port_sel ?Port_sel的针脚是什么?
与D_GPIO,GPIO和GPIO以及GPIO _REG有何不同?
非常感谢