请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DP8.363万 您好,
DP8.363万数据表说明指定该芯片符合100Base-FX光纤通信标准。 问题是我的应用程序要求达到5 km 范围,这意味着使用100Base-BX或100Base-lx标准。 IC是否可以与100Base-BX或100Base-lx模块(SFP或收发器)配合使用?
此致,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
DP8.363万数据表说明指定该芯片符合100Base-FX光纤通信标准。 问题是我的应用程序要求达到5 km 范围,这意味着使用100Base-BX或100Base-lx标准。 IC是否可以与100Base-BX或100Base-lx模块(SFP或收发器)配合使用?
此致,