Other Parts Discussed in Thread: TMDS181
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TMDS181 您好,先生:
很抱歉打扰你。
作为标题,如果我们想在 4K * 2K 60Hz上使用TMDS181,我们可以通过引脚带模式进行设置吗?
或者必须使用I2C进行控制?
以及如何设置?
顺便说一下,我们可以通过 4K * 2K 30 Hz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.