Other Parts Discussed in Thread: SN75LVCP601
您好,
我在SATA Gen 3支持方面遇到一些问题
在我的系统中,我使用具有4个端口的Kontron come模块,支持SATA Gen 1/2/3
端口0和端口1使用SN75LVCP601驱动器,在SATA Gen 1/2中工作正常,在SATA 3模式中不工作。
端口2和端口3可直接连接SSD`s,并可通过标准SATA电缆在所有速度下正常工作。
SN75LVCP601`s,位于端口0和1上,驱动器A背板,带有与背板连接的特殊SSD载波模块。
从SN75LVCP601到SSD的距离约为4英寸,从SN75LVCP601到SSD的距离约为10英寸。
有人可以为我的设置推荐重新驱动程序设置吗?
默认设置(EQ1,2 = 0 dB,DE1,2 =-4 dB, DEW1,2 = 1长)适用于Gen2,不适用于Gen 3。
此致,维克多