请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:UCC5320 你(们)好
我想知道下面电路的CA1和CA2,Rz的推荐值。 (UCC5320是S版)
(CA1和CA2是去耦电容。 应该为0.1uF?)
对于E版,我们是否可以使用E版UCC5320和上述S版电路?
此致,
山本浩二
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.