请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DS90UB913A-Q1 SNLA222 在表6中显示,要达到400kbps,SCL的“High”(高)和“Low”(低)应设置为0x32。 0x32转换为50位十进制数。 50 * 2 (用于低和高周期)*50ns (标称参考时钟周期)=总SCL周期5us。 在这种情况下,SCL频率为200kHz。 SNLA222表6中的信息是否正确?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SNLA222 在表6中显示,要达到400kbps,SCL的“High”(高)和“Low”(低)应设置为0x32。 0x32转换为50位十进制数。 50 * 2 (用于低和高周期)*50ns (标称参考时钟周期)=总SCL周期5us。 在这种情况下,SCL频率为200kHz。 SNLA222表6中的信息是否正确?