This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LMH0344:返回损耗网络说明

Guru**** 2927270 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/639125/lmh0344-return-loss-network-clarification

部件号:LMH0344
主题中讨论的其他部件:SD3GDAEVK

您好,

在交流电特性表中,注释6表示SD344评估板上并行存在3个部件(8.2 NH,0.5 pF和75欧姆)。

典型应用图3显示的是与75欧姆平行的3.9 NH。

布局示例显示输入上的5个部分(2个并联,2个串联至GND,然后1.0 UF盖至输入)

数据表的不同部分似乎相互矛盾。

您能否提供SD344评估板示意图和布局以进行说明?

谢谢!

约旦