This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:Linux
您好,
我有连接到Linux的硬件,它使用 TUSB3410。
Linux正在请求两个固件文件:
TI_USB-v10AC-P0102.FW
TI_3410.FW
我在正常下载页面上找不到这些文件:
http://www.ti.com/product/TUSB3410/toolssoftware#softTools
是否有人可以为我提供这些文件?
非常感谢和亲切问候。
您好,
此处是dmesg和syslog的输出
--
[ 17.4702万.259258</xmt-block>25.9258万 ] vhci_hcd vhci_hcd:pdev(0) rhport(2) sockpd(12)
[DevID] vhci_hcd vhci_hcd:17.4702万.259261</xmt-block>25.9261万 (6) speed (2) speed_str (全速)
[USB] 17.4702万.520592</xmt-block>52.0592万 3-3:使用vhci_hcd的全新全速设备编号4
[SetAddress] 17.4702万.644602</xmt-block>64.4602万 3-3:请求(4)至端口2
[USB] 17.4702万.715896</xmt-block>71.5896万 3-3:找到新USB设备,idVendor=10AC,idProduct=0102
[USB] 17.4702万.715900</xmt-block>71.59万 3-3:新USB设备字符串:MFR=1,产品=2,序列号=3
[USB] 17.4702万.715902</xmt-block>71.5902万 3-3:产品:TUSB3410启动设备
[德州 仪器(TI) 17.4702万.715918</xmt-block>71.5918万 3-3:制造商:
[USB] 17.4702万.715923</xmt-block>71.5923万 3-3:序列号:3410
[USB] 17.4703万.738226</xmt-block>73.8226万 usbcore:已注册的新接口驱动程序ti_USB_3410_5052</s>5052
[USB] usbserial:17.4703万.738255</xmt-block>73.8255万 串行支持已注册用于TI 3410 1端口适配器
[USB] usbserial:17.4703万.738274</xmt-block>73.8274万 串行支持已注册用于TI 5052 2端口适配器
[USB] ti_USB_3410_5052 3-35052 3-3:1.0 :检测到17.4703万.738312</xmt-block>73.8312万 3410 1端口适配器转换器
[USB] 17.4703万.738362</xmt-block>73.8362万 3-3:固件:加载ti_USB-v10ac-P0102.FW (-2)失败
[USB] 17.4703万.738378</xmt-block>73.8378万 3-3:ti_USB-v10ac-P0102.FW直接固件加载失败,错误-2
[USB] 17.4703万.738393</xmt-block>73.8393万 3-3:固件:加载ti_3410.FW (-2)失败
[USB] 17.4703万.738398</xmt-block>73.8398万 3-3:ti_3410.fw的直接固件加载失败,出现错误-2
[USB] 17.4703万.738412</xmt-block>73.8412万 ti_USB_3410_5052:5052:3-3的探测器:1.0 失败,错误-5
--
Debian 8.10
内核: Debian.0-0.BPO.4-AMD64 #1 4.9 4.9 Debian.65-3+deb9u1~bpo8+1 (2017年12月23日) x86_64 GNU/Linux