请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TSB81BA3E TSB81BA3E是否支持S200b? 客户报告其S200b设备连接不足。 我们的产品(带TSB81BA3E)在S400b和S800 (b)上运行良好,但我认为我们没有测试S200b。 谢谢你。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Roberto,
在S200b上,两个TSB81BA3E设备之间没有连接。 它们在S400b和S800b上工作正常。 这真的是一个是/否问题-- TSB81BA3E是否支持S200b?
数据表部分8.1 建议不支持此功能(98.304 ,196.608 ,393.216 ,491.52 或983.04 Mbit/s (称为S100,S200,S400,S400B或S800速度, 但Max_port_speed设置的数据表7表示可能支持此设置(允许将beta速度限制为S200或S100)。
再次感谢您的帮助,
Sung Lim