请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DS90UB947-Q1 您好,TI
你能帮我检查一下下面的块吗? 我想通过 SN65DSI85输出两个1920*720@60Hz的显示屏。当仅使用一个通道的开放式LDI (Data0~3+-和Clk+-)时,DS90UB947-Q1是否可以输出1920*720@60Hz的分辨率?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,TI
你能帮我检查一下下面的块吗? 我想通过 SN65DSI85输出两个1920*720@60Hz的显示屏。当仅使用一个通道的开放式LDI (Data0~3+-和Clk+-)时,DS90UB947-Q1是否可以输出1920*720@60Hz的分辨率?