请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他部件:TCAN1042-Q11.如何使用Tcan1042唤醒功能?
2.如果MCU和TCAN1042处于休眠状态,您能否模拟一些RX (如TCAN1042)信号输入到TCAN1042,先唤醒TCAN1042,然后唤醒MCU?
3.如果TCAN1042和MCU都处于休眠状态,它们是否开始工作?
谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.如何使用Tcan1042唤醒功能?
2.如果MCU和TCAN1042处于休眠状态,您能否模拟一些RX (如TCAN1042)信号输入到TCAN1042,先唤醒TCAN1042,然后唤醒MCU?
3.如果TCAN1042和MCU都处于休眠状态,它们是否开始工作?
谢谢你