请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DS90UB948-Q1 你(们)好
正如数据表所说:支持WUXGA (1920x1200)和1200和1080p60的像素时钟频率高达170 MHz,分辨率具有24位色深。
CAN 948和949支持2880 X 1080@50Hz,24位色深,像素色块不超过170MHz,谢谢!
此致
Jeremy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你(们)好
正如数据表所说:支持WUXGA (1920x1200)和1200和1080p60的像素时钟频率高达170 MHz,分辨率具有24位色深。
CAN 948和949支持2880 X 1080@50Hz,24位色深,像素色块不超过170MHz,谢谢!
此致
Jeremy