Other Parts Discussed in Thread: P82B96
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:P82B96 您好,先生/女士,
我们在系统上使用P82B96 I2C扩展器将传感器连接到6米远的控制器。
以下是我的规格:
SX/Sy端的电压- 3.3V
Tx/Rx端5V的电压
我需要连接两个分别以400kHz和800kHz运行的设备。 请帮助您计算相同的上拉电阻值。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.