请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:SN65HVDA100-Q1 我想确认SN65HVDA100-Q1的VOL。
在 低Vsup和低IO (例如Vsup = 5V,IO = 5mA)的情况下, VOL 与规格(Vsup = 14V,IO = 40mA)有何变化?
(例如 VOL低于规格(Vsup = 14V,IO = 40mA),依此类推)
此致,
Atsushi Yamauchi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想确认SN65HVDA100-Q1的VOL。
在 低Vsup和低IO (例如Vsup = 5V,IO = 5mA)的情况下, VOL 与规格(Vsup = 14V,IO = 40mA)有何变化?
(例如 VOL低于规格(Vsup = 14V,IO = 40mA),依此类推)
此致,
Atsushi Yamauchi