This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你(们)好
我正在寻找Display Port DP转数字视频接口转换器
此组件是否可以在如下所述的应用程序中工作?
我已查看的组件数据表:
SNx5DP149 3.4 Gbps DP++至HDMI Retimer: http://www.ti.com/lit/ds/symlink/sn75dp149.pdf
SNx5DP149 3.4 Gbps DP++到HDMI Retimer (修订版 c): http://www.ti.com/lit/ds/symlink/sn65dp149.pdf
SNx5DP159 6 Gbps DP++到HDMI Retimer http://www.ti.com/lit/ds/symlink/sn65dp159.pdf
SNx5DP159 6 Gbps DP++到HDMI Retimer http://www.ti.com/lit/ds/symlink/sn75dp159.pdf
控制:
组件名称为 :… DP++至HDMI
功能:“支持DisplayPort双模式标准版本1.1 ”
因此,支持具有活动转换器correkt的DP1.2A。
因此支持DVI-D (单链路),correkt?
SNx5DP149支持屏幕分辨率1024x768,correkt?
根据数据表,提供“温度范围工业:-40°C至85°C”,OK
Manantory 1 x主链路,AUX CH,热插拔检测,供电连接器(DP_PWR引脚)
可选:2个主链路
可选:4xMain Link
因此,我们仅使用2 av 4通道没有问题,对吗?