This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
我们正在寻找一款1394收发器均衡器,它的驱动速度超过AS5643 S200Beta 60ft标准。
TI P/N TSB41BA3B-EP (V62/0.367万-02XE)只能驱动标准距离,温度范围为-40C至110C。
请帮我找到一个类似的1394收发器,它可以驱动60英尺以上。 40C至85C的工作温度范围也应正常
谢谢!
David
所有TI PHY均设计用于短距铜缆。
据我所见,使用其它1394物理连接之一需要其它硬件;例如,IOI 说:
FW-CAT5S400允许通过5类或6类非屏蔽双绞线(UTP)电缆传输和接收1394信号。
FW-CAT5S400经过优化,可在5类或6类上以S400数据速率创建远距离IEEE 1394b-2002连接2002连接
[…]
配备多速率自适应均衡器,可恢复通过5类或6类非屏蔽双绞线(UTP)电缆接收到的IEEE标准1394b信号,速度为400 Mbits/s
FWB2GOF01是FireWire 800至GoF中继器,具有德州仪器(TI)的TSB81BA3和光纤收发器。
FWB2GOF01-MTRJ配有一个Agilent HFBR-5912E (MT-RJ)小型光纤收发器。
FWB2GOF01-LC是一个FireWire 800至GoF中继器,具有德州仪器(TI)的TSB81BA3和光纤收发器。
GOF端口是具有LC双工连接器的千兆位以太网850nm VCSEL (多模)收发器。
利用IEEE1394 PHY和光纤收发器,FWB2GOF01-LC能够通过长度高达500米的LC/LC光纤电缆发送IEEE1394信号!