Other Parts Discussed in Thread: TCA9535
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TCA9535 您好,
将TCA9535的中断引脚上拉至与VDD不同的电压时是否有任何问题?
我想为TCA9535提供5V电源,并在中断引脚上使用3V3上拉式。

谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.