请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TDP0604 大家好、
TDP0604是否可与1.8V HDMI 输入搭配使用? 它具有内部3.3V 电压偏置、因此我认为1.8V 输入可能不符合要求。 如果是、我们是否有任何可接受1.8V 输入信号的 HDMI 转接驱动器/重定时器?

谢谢!
罗伊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.