请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:SN65DSI84 尊敬的专家
现在、SN65DSI84有两个问题、如下所示:
配置 SN65DSI84寄存器后、LCD 屏幕会显示、但 E5寄存器的校验值不是00、而是81。 您能否帮助解释81代表什么?

SN65DSI84偶尔不会有 LVDS 信号输出(概率约为1%)、导致 LCD 屏幕上不显示。 DSI 信号输入已确认、您能否帮助分析问题出在哪?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.