主题中讨论的其他器件:DP83869
大家好、
客户 的 iMX6 RGMII 接口为1.5V 逻辑、无需电平位移即可直接通信吗?
如果我的理解是正确的、则 VDDIO 具有内部 LDO 1.8V 选择。
因此 、参考 VDDIO x 0.35和 VDDIO x 0.65、即0.63V 和1.17V。 我觉得还可以,但是要仔细检查一下
谢谢!
Andrew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.