主题中讨论的其他器件: SN65DSI85
您好!
SN65DSI86中的寄存器0x93可以启用展频。
最大值为5000ppm。 这大约是0.5%、对吧?
如何实现2%的展频?
我可以使用具有2%展频的外部 REFCLK 来实现此目的吗? 有副作用吗?
BR、
弗兰克
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.