Other Parts Discussed in Thread: XIO2001
1、XIO2001连接到 PCI 插槽1的时钟信号 pciclk1的路由长度是否应等于 XIO2001连接到 PCI 插槽2的时钟信号 pciclk2的路由长度?
2、PCI 插槽1中与时钟信号 pciclk1同步的信号(如 ad31-0信号)是否具有相同的长度?
3、Fbclk 布线长度要求?
4、PCI 插槽的时钟信号 pciclk 是否比 ad32-0信号的长度短2.5英寸?
谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: XIO2001
1、XIO2001连接到 PCI 插槽1的时钟信号 pciclk1的路由长度是否应等于 XIO2001连接到 PCI 插槽2的时钟信号 pciclk2的路由长度?
2、PCI 插槽1中与时钟信号 pciclk1同步的信号(如 ad31-0信号)是否具有相同的长度?
3、Fbclk 布线长度要求?
4、PCI 插槽的时钟信号 pciclk 是否比 ad32-0信号的长度短2.5英寸?
谢谢你

非常感谢您的回复。 我的问题是:(如上图所示)
1、pciclk1的长度 L1是否必须等于 pciclk2的长度 L2?
2、pciclk1的长度 L1是否必须等于 ad32-0的长度 L3? 允许的偏差 L1-L3是多少?
3、pciclk1的长度 L2是否必须等于 ad32-0的长度 L3+L4? 允许 的偏差 L2-(L3+L4)是多少?
4、Fbclk 路由长度 L1 pciclk1的长度与 L2 pciclk2的长度之间的 L5关系? L5 = L2+2500mil?
非常感谢!