请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS65988 主题中讨论的其他器件: TPS55288
我需要使 PDO1的电压输出为5.25V、我需要如何操作它?
我使用 TPS65988和 TPS55288连接 I2C1。 TPS65988的 PDO1设置为5V/3A、但我需要 PDO1实际输出5.25V。 我应该怎么做?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.