请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:SN65DSI83 尊敬的:
我对 SN65DSI83 REFCLK 的上升和下降时间有疑问。
SN65DSI83的 REFCLK 的上升和下降时间是否为10%至90%?
还是20%到80%?
(TR/TF 最小值100ps 最大值1ns)
此致、
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.