Other Parts Discussed in Thread: DS25BR100
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DS25BR100 您好!
我正在寻找 具有 Ta:105C 或汽车级的600Mbps LVDS 缓冲器。
例如、如果 DS25BR100覆盖高达105°C、则这可能是一种理想的解决方案。
提前感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.