请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TCA9548A 主题中讨论的其他器件:TPS3808
您好!
我的设计中有一个全局复位信号(TPS3808)、拉至1.8V、我想将其连接到 TAC9548A。
我需要电平转换、还是可以连接 VCC、A0-A2并复位至1.8V 电平功率/信号?
主器件侧为3.3V、而从器件侧混合了3.3V 和1.8V。
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.