请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS2553 大家好、
TPS2553是恒定电流限制版本、我们知道、当电流刚好超过限制时、输出电压应首先下降。
但为什么在发生电流限制事件时提供保护?
测试方法:
VIN=5.2V;Vout:5V、 Eload CC 模式下灌电流500mA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.