Other Parts Discussed in Thread: SN75DP159
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:SN75DP159 尊敬的团队:
数据表显示、DP159可以支持每种颜色的超高清4K 60Hz 8位高分辨率视频。
到目前为止、我的客户需要支持4K 60Hz 10位色深的转接驱动器。
那么、他们是否可以使用 DP159?
谢谢你。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.