Other Parts Discussed in Thread: ISO1541
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:ISO1541 我正在查找 ISO1541上的可靠性数据,但在您的站点上找不到这些数据。
您能将我指向网页、还是提供此数据? 我特别想在50°和80°的结点寻找 MTBF/FPMH 数字,以获得60%的置信度。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.