Other Parts Discussed in Thread: ISO5851, ISO5451
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:ISO5851 主题中讨论的其他器件: ISO5451
尊敬的同事:
对于 ISO5851或 ISO5451、有0V 电压来开关 MOSFET 还是真的需要负电压来关闭 MOSFET?
非常感谢、
传真
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.