请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TS3DV642 您好、先生、
我的客户将使用 TS3DV642来执行 DPv1.4级联应用、分辨率为4K 120Hz 或8K 30Hz、如下图所示。

输入电缆使用标准类型、并在第1个 TS3DV642的输入和第2个 TS3DV642的输出上使用过孔至信号平面。
为了确保信号的完整性、它们能否移除第一个 TS3DV642输入上的所有 DPv1.4重定时器器件?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.