请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:ISO5852S ISO5852S 的输出拉电流容量为2.5A、我们能否在输出端使用 MOSFET 升压器来增加输出拉电流和灌电流容量?
在 ISO5852晶体管的应用手册中、该晶体管用于电流升压、可在高达50kHz 的开关频率下使用、峰值拉电流和灌电流为50A?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.