Other Parts Discussed in Thread: ULN2003A, ULN2003B
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:ULN2003B 主题中讨论的其他器件:ULN2003A、
您能告诉我将输出从导通状态更改为关断状态的最小输入电压吗?
ULN2003A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
数据表的第8.3节指出:
GPIO 电压 kΩ 连接在前置驱动器达林顿 NPN 输入和基极之间的2.7k Ω 电阻转换为基极电流。 kΩ kΩ NPN 基极和发射极之间的7.2k Ω 和3k Ω 电阻充当下拉电阻、并抑制输入端可能出现的泄漏量。
第6.6节 µA 输入电流应小于30 μ A。 kΩ 输入和接地之间约为12.9 μ A、这对应于大约0.39V。(这适用于半毫安的集电极电流;您需要更低的电流。)