Other Parts Discussed in Thread: DP83867E
我们目前正在初始化 DP83867E 以太网接口(SGMII)。 不过、尽管使用了提供的驱动程序(此驱动程序与 RGMII 驱动程序类似、我们需要 SGMII 驱动程序)并按照随附的原理图中的说明配置了 strap 配置选项、但在建立与网络的连接时仍然会遇到困难。 我们恳请您的协助和指导、以确定任何必要的 modificatione2e.ti.com/.../readme.docxs、从而确保其适当的 functionality.e2e.ti.com/.../Ethernet-PHY.pdf
/*
* Driver for the Texas Instruments DP83867 PHY
*
* Copyright (C) 2015 Texas Instruments Inc.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License as published by
* the Free Software Foundation; either version 2 of the License.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*/
#include <linux/ethtool.h>
#include <linux/kernel.h>
#include <linux/mii.h>
#include <linux/module.h>
#include <linux/of.h>
#include <linux/phy.h>
#include <dt-bindings/net/ti-dp83867.h>
#define DP83867_PHY_ID 0x2000a231
#define DP83867_DEVADDR 0x1f
#define MII_DP83867_PHYCTRL 0x10
#define MII_DP83867_MICR 0x12
#define MII_DP83867_ISR 0x13
#define DP83867_CTRL 0x1f
#define DP83867_CFG3 0x1e
/* Extended Registers */
#define DP83867_CFG4 0x0031
#define DP83867_RGMIICTL 0x0032
#define DP83867_STRAP_STS1 0x006E
#define DP83867_RGMIIDCTL 0x0086
#define DP83867_IO_MUX_CFG 0x0170
#define DP83867_SW_RESET BIT(15)
#define DP83867_SW_RESTART BIT(14)
/* MICR Interrupt bits */
#define MII_DP83867_MICR_AN_ERR_INT_EN BIT(15)
#define MII_DP83867_MICR_SPEED_CHNG_INT_EN BIT(14)
#define MII_DP83867_MICR_DUP_MODE_CHNG_INT_EN BIT(13)
#define MII_DP83867_MICR_PAGE_RXD_INT_EN BIT(12)
#define MII_DP83867_MICR_AUTONEG_COMP_INT_EN BIT(11)
#define MII_DP83867_MICR_LINK_STS_CHNG_INT_EN BIT(10)
#define MII_DP83867_MICR_FALSE_CARRIER_INT_EN BIT(8)
#define MII_DP83867_MICR_SLEEP_MODE_CHNG_INT_EN BIT(4)
#define MII_DP83867_MICR_WOL_INT_EN BIT(3)
#define MII_DP83867_MICR_XGMII_ERR_INT_EN BIT(2)
#define MII_DP83867_MICR_POL_CHNG_INT_EN BIT(1)
#define MII_DP83867_MICR_JABBER_INT_EN BIT(0)
/* RGMIICTL bits */
#define DP83867_RGMII_TX_CLK_DELAY_EN BIT(1)
#define DP83867_RGMII_RX_CLK_DELAY_EN BIT(0)
/* STRAP_STS1 bits */
#define DP83867_STRAP_STS1_RESERVED BIT(11)
/* PHY CTRL bits */
#define DP83867_PHYCR_FIFO_DEPTH_SHIFT 14
#define DP83867_PHYCR_FIFO_DEPTH_MASK (3 << 14)
#define DP83867_PHYCR_RESERVED_MASK BIT(11)
/* RGMIIDCTL bits */
#define DP83867_RGMII_TX_CLK_DELAY_SHIFT 4
/* IO_MUX_CFG bits */
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL 0x1f
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_MAX 0x0
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_MIN 0x1f
/* CFG4 bits */
#define DP83867_CFG4_PORT_MIRROR_EN BIT(0)
enum {
DP83867_PORT_MIRROING_KEEP,
DP83867_PORT_MIRROING_EN,
DP83867_PORT_MIRROING_DIS,
};
struct dp83867_private {
int rx_id_delay;
int tx_id_delay;
int fifo_depth;
int io_impedance;
int port_mirroring;
bool rxctrl_strap_quirk;
};
static int dp83867_ack_interrupt(struct phy_device *phydev)
{
int err = phy_read(phydev, MII_DP83867_ISR);
if (err < 0)
return err;
return 0;
}
static int dp83867_config_intr(struct phy_device *phydev)
{
int micr_status;
if (phydev->interrupts == PHY_INTERRUPT_ENABLED) {
micr_status = phy_read(phydev, MII_DP83867_MICR);
if (micr_status < 0)
return micr_status;
micr_status |=
(MII_DP83867_MICR_AN_ERR_INT_EN |
MII_DP83867_MICR_SPEED_CHNG_INT_EN |
MII_DP83867_MICR_AUTONEG_COMP_INT_EN |
MII_DP83867_MICR_LINK_STS_CHNG_INT_EN |
MII_DP83867_MICR_DUP_MODE_CHNG_INT_EN |
MII_DP83867_MICR_SLEEP_MODE_CHNG_INT_EN);
return phy_write(phydev, MII_DP83867_MICR, micr_status);
}
micr_status = 0x0;
return phy_write(phydev, MII_DP83867_MICR, micr_status);
}
static int dp83867_config_port_mirroring(struct phy_device *phydev)
{
struct dp83867_private *dp83867 =
(struct dp83867_private *)phydev->priv;
u16 val;
val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4);
if (dp83867->port_mirroring == DP83867_PORT_MIRROING_EN)
val |= DP83867_CFG4_PORT_MIRROR_EN;
else
val &= ~DP83867_CFG4_PORT_MIRROR_EN;
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4, val);
return 0;
}
#ifdef CONFIG_OF_MDIO
static int dp83867_of_init(struct phy_device *phydev)
{
struct dp83867_private *dp83867 = phydev->priv;
struct device *dev = &phydev->mdio.dev;
struct device_node *of_node = dev->of_node;
int ret;
if (!of_node)
return -ENODEV;
dp83867->io_impedance = -EINVAL;
/* Optional configuration */
if (of_property_read_bool(of_node, "ti,max-output-impedance"))
dp83867->io_impedance = DP83867_IO_MUX_CFG_IO_IMPEDANCE_MAX;
else if (of_property_read_bool(of_node, "ti,min-output-impedance"))
dp83867->io_impedance = DP83867_IO_MUX_CFG_IO_IMPEDANCE_MIN;
dp83867->rxctrl_strap_quirk = of_property_read_bool(of_node,
"ti,dp83867-rxctrl-strap-quirk");
ret = of_property_read_u32(of_node, "ti,rx-internal-delay",
&dp83867->rx_id_delay);
if (ret &&
(phydev->interface == PHY_INTERFACE_MODE_RGMII_ID ||
phydev->interface == PHY_INTERFACE_MODE_RGMII_RXID))
return ret;
ret = of_property_read_u32(of_node, "ti,tx-internal-delay",
&dp83867->tx_id_delay);
if (ret &&
(phydev->interface == PHY_INTERFACE_MODE_RGMII_ID ||
phydev->interface == PHY_INTERFACE_MODE_RGMII_TXID))
return ret;
if (of_property_read_bool(of_node, "enet-phy-lane-swap"))
dp83867->port_mirroring = DP83867_PORT_MIRROING_EN;
if (of_property_read_bool(of_node, "enet-phy-lane-no-swap"))
dp83867->port_mirroring = DP83867_PORT_MIRROING_DIS;
return of_property_read_u32(of_node, "ti,fifo-depth",
&dp83867->fifo_depth);
}
#else
static int dp83867_of_init(struct phy_device *phydev)
{
return 0;
}
#endif /* CONFIG_OF_MDIO */
static int dp83867_config_init(struct phy_device *phydev)
{
struct dp83867_private *dp83867;
int ret, val, bs;
u16 delay;
if (!phydev->priv) {
dp83867 = devm_kzalloc(&phydev->dev, sizeof(*dp83867),
//dp83867 = devm_kzalloc(&phydev->mdio.dev, sizeof(*dp83867),
GFP_KERNEL);
if (!dp83867)
return -ENOMEM;
phydev->priv = dp83867;
ret = dp83867_of_init(phydev);
if (ret)
return ret;
} else {
dp83867 = (struct dp83867_private *)phydev->priv;
}
/* RX_DV/RX_CTRL strapped in mode 1 or mode 2 workaround */
if (dp83867->rxctrl_strap_quirk) {
val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4);
val &= ~BIT(7);
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4, val);
}
printk("********** %s %d\n",__func__,__LINE__);
#if 0
if (phy_interface_is_rgmii(phydev)) {
val = phy_read(phydev, MII_DP83867_PHYCTRL);
if (val < 0)
return val;
val &= ~DP83867_PHYCR_FIFO_DEPTH_MASK;
val |= (dp83867->fifo_depth << DP83867_PHYCR_FIFO_DEPTH_SHIFT);
/* The code below checks if "port mirroring" N/A MODE4 has been
* enabled during power on bootstrap.
*
* Such N/A mode enabled by mistake can put PHY IC in some
* internal testing mode and disable RGMII transmission.
*
* In this particular case one needs to check STRAP_STS1
* register's bit 11 (marked as RESERVED).
*/
bs = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_STRAP_STS1);
if (bs & DP83867_STRAP_STS1_RESERVED)
val &= ~DP83867_PHYCR_RESERVED_MASK;
ret = phy_write(phydev, MII_DP83867_PHYCTRL, val);
if (ret)
return ret;
/* Set up RGMII delays */
val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_RGMIICTL);
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_ID)
val |= (DP83867_RGMII_TX_CLK_DELAY_EN | DP83867_RGMII_RX_CLK_DELAY_EN);
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_TXID)
val |= DP83867_RGMII_TX_CLK_DELAY_EN;
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_RXID)
val |= DP83867_RGMII_RX_CLK_DELAY_EN;
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_RGMIICTL, val);
delay = (dp83867->rx_id_delay |
(dp83867->tx_id_delay << DP83867_RGMII_TX_CLK_DELAY_SHIFT));
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_RGMIIDCTL,
delay);
if (dp83867->io_impedance >= 0) {
val = phy_read_mmd(phydev, DP83867_DEVADDR,
DP83867_IO_MUX_CFG);
val &= ~DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL;
val |= dp83867->io_impedance &
DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL;
phy_write_mmd(phydev, DP83867_DEVADDR,
DP83867_IO_MUX_CFG, val);
}
}
#endif
/* Enable Interrupt output INT_OE in CFG3 register */
if (phy_interrupt_is_valid(phydev)) {
val = phy_read(phydev, DP83867_CFG3);
val |= BIT(7);
phy_write(phydev, DP83867_CFG3, val);
}
if (dp83867->port_mirroring != DP83867_PORT_MIRROING_KEEP)
dp83867_config_port_mirroring(phydev);
return 0;
}
static int dp83867_phy_reset(struct phy_device *phydev)
{
int err;
err = phy_write(phydev, DP83867_CTRL, DP83867_SW_RESET);
if (err < 0)
return err;
return dp83867_config_init(phydev);
}
static struct phy_driver dp83867_driver[] = {
{
.phy_id = DP83867_PHY_ID,
.phy_id_mask = 0xfffffff0,
.name = "TI DP83867",
.features = PHY_GBIT_FEATURES,
.flags = PHY_HAS_INTERRUPT,
.config_init = dp83867_config_init,
.soft_reset = dp83867_phy_reset,
/* IRQ related */
.ack_interrupt = dp83867_ack_interrupt,
.config_intr = dp83867_config_intr,
.config_aneg = genphy_config_aneg,
.read_status = genphy_read_status,
.suspend = genphy_suspend,
.resume = genphy_resume,
},
};
//module_phy_driver(dp83867_driver);
static int __init dp83867_init(void)
{
return phy_driver_register(&dp83867_driver);
}
static void __exit dp83867_exit(void)
{
// dp83640_free_clocks();
phy_driver_unregister(&dp83867_driver);
}
module_init(dp83867_init);
module_exit(dp83867_exit);
static struct mdio_device_id __maybe_unused dp83867_tbl[] = {
{ DP83867_PHY_ID, 0xfffffff0 },
{ }
};
MODULE_DEVICE_TABLE(mdio, dp83867_tbl);
MODULE_DESCRIPTION("Texas Instruments DP83867 PHY driver");
MODULE_AUTHOR("Dan Murphy <dmurphy@ti.com");
MODULE_LICENSE("GPL");

以下是更新后的观察结果。