This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DP83867E:SGMII 驱动程序支持

Guru**** 2782575 points

Other Parts Discussed in Thread: DP83867E

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1279404/dp83867e-sgmii-driver-support

器件型号:DP83867E

我们目前正在初始化 DP83867E 以太网接口(SGMII)。 不过、尽管使用了提供的驱动程序(此驱动程序与 RGMII 驱动程序类似、我们需要 SGMII 驱动程序)并按照随附的原理图中的说明配置了 strap 配置选项、但在建立与网络的连接时仍然会遇到困难。 我们恳请您的协助和指导、以确定任何必要的 modificatione2e.ti.com/.../readme.docxs、从而确保其适当的 functionality.e2e.ti.com/.../Ethernet-PHY.pdf

/*
 * Driver for the Texas Instruments DP83867 PHY
 *
 * Copyright (C) 2015 Texas Instruments Inc.
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation; either version 2 of the License.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 */

#include <linux/ethtool.h>
#include <linux/kernel.h>
#include <linux/mii.h>
#include <linux/module.h>
#include <linux/of.h>
#include <linux/phy.h>

#include <dt-bindings/net/ti-dp83867.h>

#define DP83867_PHY_ID		0x2000a231
#define DP83867_DEVADDR		0x1f

#define MII_DP83867_PHYCTRL	0x10
#define MII_DP83867_MICR	0x12
#define MII_DP83867_ISR		0x13
#define DP83867_CTRL		0x1f
#define DP83867_CFG3		0x1e

/* Extended Registers */
#define DP83867_CFG4            0x0031
#define DP83867_RGMIICTL	0x0032
#define DP83867_STRAP_STS1	0x006E
#define DP83867_RGMIIDCTL	0x0086
#define DP83867_IO_MUX_CFG	0x0170

#define DP83867_SW_RESET	BIT(15)
#define DP83867_SW_RESTART	BIT(14)

/* MICR Interrupt bits */
#define MII_DP83867_MICR_AN_ERR_INT_EN		BIT(15)
#define MII_DP83867_MICR_SPEED_CHNG_INT_EN	BIT(14)
#define MII_DP83867_MICR_DUP_MODE_CHNG_INT_EN	BIT(13)
#define MII_DP83867_MICR_PAGE_RXD_INT_EN	BIT(12)
#define MII_DP83867_MICR_AUTONEG_COMP_INT_EN	BIT(11)
#define MII_DP83867_MICR_LINK_STS_CHNG_INT_EN	BIT(10)
#define MII_DP83867_MICR_FALSE_CARRIER_INT_EN	BIT(8)
#define MII_DP83867_MICR_SLEEP_MODE_CHNG_INT_EN	BIT(4)
#define MII_DP83867_MICR_WOL_INT_EN		BIT(3)
#define MII_DP83867_MICR_XGMII_ERR_INT_EN	BIT(2)
#define MII_DP83867_MICR_POL_CHNG_INT_EN	BIT(1)
#define MII_DP83867_MICR_JABBER_INT_EN		BIT(0)

/* RGMIICTL bits */
#define DP83867_RGMII_TX_CLK_DELAY_EN		BIT(1)
#define DP83867_RGMII_RX_CLK_DELAY_EN		BIT(0)

/* STRAP_STS1 bits */
#define DP83867_STRAP_STS1_RESERVED		BIT(11)

/* PHY CTRL bits */
#define DP83867_PHYCR_FIFO_DEPTH_SHIFT		14
#define DP83867_PHYCR_FIFO_DEPTH_MASK		(3 << 14)
#define DP83867_PHYCR_RESERVED_MASK		BIT(11)

/* RGMIIDCTL bits */
#define DP83867_RGMII_TX_CLK_DELAY_SHIFT	4

/* IO_MUX_CFG bits */
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL	0x1f

#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_MAX	0x0
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_MIN	0x1f

/* CFG4 bits */
#define DP83867_CFG4_PORT_MIRROR_EN              BIT(0)

enum {
	DP83867_PORT_MIRROING_KEEP,
	DP83867_PORT_MIRROING_EN,
	DP83867_PORT_MIRROING_DIS,
};

struct dp83867_private {
	int rx_id_delay;
	int tx_id_delay;
	int fifo_depth;
	int io_impedance;
	int port_mirroring;
	bool rxctrl_strap_quirk;
};

static int dp83867_ack_interrupt(struct phy_device *phydev)
{
	int err = phy_read(phydev, MII_DP83867_ISR);

	if (err < 0)
		return err;

	return 0;
}

static int dp83867_config_intr(struct phy_device *phydev)
{
	int micr_status;

	if (phydev->interrupts == PHY_INTERRUPT_ENABLED) {
		micr_status = phy_read(phydev, MII_DP83867_MICR);
		if (micr_status < 0)
			return micr_status;

		micr_status |=
			(MII_DP83867_MICR_AN_ERR_INT_EN |
			MII_DP83867_MICR_SPEED_CHNG_INT_EN |
			MII_DP83867_MICR_AUTONEG_COMP_INT_EN |
			MII_DP83867_MICR_LINK_STS_CHNG_INT_EN |
			MII_DP83867_MICR_DUP_MODE_CHNG_INT_EN |
			MII_DP83867_MICR_SLEEP_MODE_CHNG_INT_EN);

		return phy_write(phydev, MII_DP83867_MICR, micr_status);
	}

	micr_status = 0x0;
	return phy_write(phydev, MII_DP83867_MICR, micr_status);
}

static int dp83867_config_port_mirroring(struct phy_device *phydev)
{
	struct dp83867_private *dp83867 =
		(struct dp83867_private *)phydev->priv;
	u16 val;

	val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4);

	if (dp83867->port_mirroring == DP83867_PORT_MIRROING_EN)
		val |= DP83867_CFG4_PORT_MIRROR_EN;
	else
		val &= ~DP83867_CFG4_PORT_MIRROR_EN;

	phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4, val);

	return 0;
}

#ifdef CONFIG_OF_MDIO
static int dp83867_of_init(struct phy_device *phydev)
{
	struct dp83867_private *dp83867 = phydev->priv;
	struct device *dev = &phydev->mdio.dev;
	struct device_node *of_node = dev->of_node;
	int ret;

	if (!of_node)
		return -ENODEV;

	dp83867->io_impedance = -EINVAL;

	/* Optional configuration */
	if (of_property_read_bool(of_node, "ti,max-output-impedance"))
		dp83867->io_impedance = DP83867_IO_MUX_CFG_IO_IMPEDANCE_MAX;
	else if (of_property_read_bool(of_node, "ti,min-output-impedance"))
		dp83867->io_impedance = DP83867_IO_MUX_CFG_IO_IMPEDANCE_MIN;

	dp83867->rxctrl_strap_quirk = of_property_read_bool(of_node,
					"ti,dp83867-rxctrl-strap-quirk");

	ret = of_property_read_u32(of_node, "ti,rx-internal-delay",
				   &dp83867->rx_id_delay);
	if (ret &&
	    (phydev->interface == PHY_INTERFACE_MODE_RGMII_ID ||
	     phydev->interface == PHY_INTERFACE_MODE_RGMII_RXID))
		return ret;

	ret = of_property_read_u32(of_node, "ti,tx-internal-delay",
				   &dp83867->tx_id_delay);
	if (ret &&
	    (phydev->interface == PHY_INTERFACE_MODE_RGMII_ID ||
	     phydev->interface == PHY_INTERFACE_MODE_RGMII_TXID))
		return ret;

	if (of_property_read_bool(of_node, "enet-phy-lane-swap"))
		dp83867->port_mirroring = DP83867_PORT_MIRROING_EN;

	if (of_property_read_bool(of_node, "enet-phy-lane-no-swap"))
		dp83867->port_mirroring = DP83867_PORT_MIRROING_DIS;

	return of_property_read_u32(of_node, "ti,fifo-depth",
				   &dp83867->fifo_depth);
}
#else
static int dp83867_of_init(struct phy_device *phydev)
{
	return 0;
}
#endif /* CONFIG_OF_MDIO */

static int dp83867_config_init(struct phy_device *phydev)
{
	struct dp83867_private *dp83867;
	int ret, val, bs;
	u16 delay;

	if (!phydev->priv) {
		dp83867 = devm_kzalloc(&phydev->dev, sizeof(*dp83867),

		//dp83867 = devm_kzalloc(&phydev->mdio.dev, sizeof(*dp83867),
				       GFP_KERNEL);
		if (!dp83867)
			return -ENOMEM;

		phydev->priv = dp83867;
		ret = dp83867_of_init(phydev);
		if (ret)
			return ret;
	} else {
		dp83867 = (struct dp83867_private *)phydev->priv;
	}

	/* RX_DV/RX_CTRL strapped in mode 1 or mode 2 workaround */
	if (dp83867->rxctrl_strap_quirk) {
		val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4);
		val &= ~BIT(7);
		phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4, val);
	}


    printk("********** %s   %d\n",__func__,__LINE__);
#if 0
	if (phy_interface_is_rgmii(phydev)) {
		val = phy_read(phydev, MII_DP83867_PHYCTRL);
		if (val < 0)
			return val;
		val &= ~DP83867_PHYCR_FIFO_DEPTH_MASK;
		val |= (dp83867->fifo_depth << DP83867_PHYCR_FIFO_DEPTH_SHIFT);

		/* The code below checks if "port mirroring" N/A MODE4 has been
		 * enabled during power on bootstrap.
		 *
		 * Such N/A mode enabled by mistake can put PHY IC in some
		 * internal testing mode and disable RGMII transmission.
		 *
		 * In this particular case one needs to check STRAP_STS1
		 * register's bit 11 (marked as RESERVED).
		 */

		bs = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_STRAP_STS1);
		if (bs & DP83867_STRAP_STS1_RESERVED)
			val &= ~DP83867_PHYCR_RESERVED_MASK;

		ret = phy_write(phydev, MII_DP83867_PHYCTRL, val);
		if (ret)
			return ret;

		/* Set up RGMII delays */
		val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_RGMIICTL);

		if (phydev->interface == PHY_INTERFACE_MODE_RGMII_ID)
			val |= (DP83867_RGMII_TX_CLK_DELAY_EN | DP83867_RGMII_RX_CLK_DELAY_EN);

		if (phydev->interface == PHY_INTERFACE_MODE_RGMII_TXID)
			val |= DP83867_RGMII_TX_CLK_DELAY_EN;

		if (phydev->interface == PHY_INTERFACE_MODE_RGMII_RXID)
			val |= DP83867_RGMII_RX_CLK_DELAY_EN;

		phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_RGMIICTL, val);

		delay = (dp83867->rx_id_delay |
			(dp83867->tx_id_delay << DP83867_RGMII_TX_CLK_DELAY_SHIFT));

		phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_RGMIIDCTL,
			      delay);

		if (dp83867->io_impedance >= 0) {
			val = phy_read_mmd(phydev, DP83867_DEVADDR,
					   DP83867_IO_MUX_CFG);

			val &= ~DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL;
			val |= dp83867->io_impedance &
			       DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL;

			phy_write_mmd(phydev, DP83867_DEVADDR,
				      DP83867_IO_MUX_CFG, val);
		}
	}
#endif

	/* Enable Interrupt output INT_OE in CFG3 register */
	if (phy_interrupt_is_valid(phydev)) {
		val = phy_read(phydev, DP83867_CFG3);
		val |= BIT(7);
		phy_write(phydev, DP83867_CFG3, val);
	}

	if (dp83867->port_mirroring != DP83867_PORT_MIRROING_KEEP)
		dp83867_config_port_mirroring(phydev);

	return 0;
}

static int dp83867_phy_reset(struct phy_device *phydev)
{
	int err;

	err = phy_write(phydev, DP83867_CTRL, DP83867_SW_RESET);
	if (err < 0)
		return err;

	return dp83867_config_init(phydev);
}

static struct phy_driver dp83867_driver[] = {
	{
		.phy_id		= DP83867_PHY_ID,
		.phy_id_mask	= 0xfffffff0,
		.name		= "TI DP83867",
		.features	= PHY_GBIT_FEATURES,
		.flags		= PHY_HAS_INTERRUPT,

		.config_init	= dp83867_config_init,
		.soft_reset	= dp83867_phy_reset,

		/* IRQ related */
		.ack_interrupt	= dp83867_ack_interrupt,
		.config_intr	= dp83867_config_intr,

		.config_aneg	= genphy_config_aneg,
		.read_status	= genphy_read_status,
		.suspend	= genphy_suspend,
		.resume		= genphy_resume,
	},
};

//module_phy_driver(dp83867_driver);

static int __init dp83867_init(void)
{
	return phy_driver_register(&dp83867_driver);
}

static void __exit dp83867_exit(void)
{
//	dp83640_free_clocks();
	phy_driver_unregister(&dp83867_driver);
}

module_init(dp83867_init);
module_exit(dp83867_exit);


static struct mdio_device_id __maybe_unused dp83867_tbl[] = {
	{ DP83867_PHY_ID, 0xfffffff0 },
	{ }
};

MODULE_DEVICE_TABLE(mdio, dp83867_tbl);

MODULE_DESCRIPTION("Texas Instruments DP83867 PHY driver");
MODULE_AUTHOR("Dan Murphy <dmurphy@ti.com");
MODULE_LICENSE("GPL");

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好、Suhas

    我将对此进行研究、并在几天后提供最新信息。

    此致、

    梅利萨

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Suhas:

    您从何处收到此驱动程序? 我们网站上为 DP83867提供的最新 Linux 驱动程序支持 SGMII。

    您可以访问以下网站来查找我们的 Linux 驱动程序: 以太网软件驱动程序或库| TI.com 

    向下滚动至"DP.83867 Linux Driver"、然后点击红色按钮"查看合作伙伴站点"。

    此致、

    梅利萨

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

      以下是更新后的观察结果。

    使用的 MAC 接口: SGMII

    问题说明:我们目前在通过以太网接口建立通信方面遇到挑战。

    观察结果:我们无法 ping 任何地址、即使是在一对一连接场景中也是如此。

    器件退出复位条件后、我们注意到我们收到了 SGMII 信号、如随附图像中所示。 此外、我们观察到 RX_CLK 信号在某个2.5 MHz 频率下脉动、即使在没有连接电缆的情况下也是如此。 建立1Gbps 链路后、尽管我们没有采用125 MHz 接口、但该链路会转换为 RGMII。 不过、SGMII 信号的状态保持不变。 我们恳请你协助解决这一问题。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Suhas:

    您是否可以提供寄存器 0x6E、0x37和0xD3?

    您可以尝试在0x31中调整 SGMII 自动协商计时器、或者直接禁用0x14中的自动协商。  

    此外、请确认已正确配置 SGMII 自举。 SGMII strap 配置为引脚47、您可以在 DP83867E 数据表的第8.5.1节" Strap 配置"中了解更多信息。

    此致、

    梅利萨