主题中讨论的其他器件:DP83TC811
我根据文档 snla276将 DP83TC811配置为测试模式1、但输出速度应为10BASE-T1。 是否可以为100BASE-T1提供 REG 设置?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我根据文档 snla276将 DP83TC811配置为测试模式1、但输出速度应为10BASE-T1。 是否可以为100BASE-T1提供 REG 设置?
根据100BASE-T1 (IEEE802.3bw)规范和测试标准、规范屏幕截图中给出了测试模式1的定义:因此、测试模式1的周期=>34+1/34-1符号~ 40+1/40-1符号、符号速率100BASE-T1为66.66 MHz = 15ns。 测试模式1的正确周期为(34*2) 15ns = 1.02 µs ~(402)* 15ns = 1.2 µs、处于 Tektronix 软件检查范围内。