Other Parts Discussed in Thread: AM26LV31E
主题中讨论的其他器件:AM26LV31E
工具与软件:
这两款器件的数据表没有提及对 V.11/X.27的任何符合性。。。
客户想知道这两个器件是否隐式符合这些标准、而不在数据表中引用任何内容?
如果没有、哪些现代器件符合这些标准?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、Walter、
Clemens 是正确的、V.11/X.27只需参阅 RS -422标准。 RS485标准和 RS -422标准之间的主要区别在于负载要求两端的压降以及总线上器件数量的限制(32个单位负载对最大10个)。 RS485通常使用60欧姆的端接电阻器、但该标准要求您假设它是54欧姆(负方向容差为10%)。 54欧姆负载上的压降为最小值1.5V。 对于 RS 至422、我相信它们使用100欧姆、最低电压为2.2V。 RS -485的定义比 RS -422更难通过、因此默认情况下、RS485驱动器能够驱动100 Ω 负载、并满足 RS -422对端接电阻器两端电压的要求。
简单来说、如果满足 RS 至485标准、那么满足 RS 至422标准。
-鲍比