This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 数字隔离器,而不是光耦合器

Guru**** 2963370 points

Other Parts Discussed in Thread: ISO1212, ISO1211

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1092830/digital-isolator-instead-of-optocoupler

主题中讨论的其他部件:ISO1212, ISO1211

大家好,

目前,我们正在使用光耦合器HCPL-063L来隔离我们的数字输入。

我们的输入信号为24V。

您是否有支持24V输入和3.3V输出的数字隔离器解决方案?

从输入端,我们只有24V信号和GND,并且没有电源。

如果您没有可直接支持24V的数字隔离器,那么可能是将24V电平转换器组合到3.3V,然后再组合具有集成电源的数字隔离器?

此致,

David。