请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:ISO1042 主题中讨论的其他器件: ISO1050
客户对 ISO1050和 ISO1042之间的差异很好奇。 µs ISO1050中的 CMTI 为50kV/μ s、µs ISO1042有没有不同的技术可将 CMTI 提高到100kV/μ s?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.