Other Parts Discussed in Thread: ISO1450
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:ISO1450 大家好、团队成员
请告诉我们在以下特定条件下 PD 的功率。
ISO1450的 Vcc1=3.3 Vcc2=5V、Tj=125℃频率= 50MHz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.