请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:ISOW7841 1.我测试 ADUM6400在电路上可以正常使用。当我测试 ISOW7841使用相同电路时、Viso 可能会拉低至1V、测量电流为80mA、不能超过130mA、但在断开负载连接时可以使用、请提供一些建议、谢谢
VBUS 输入为5V/1A、Viso 为3.3V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.