Other Parts Discussed in Thread: ISO1044, ISOW1044
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:ISO1044 主题中讨论的其他器件: ISOW1044
您好
目前正在对我们的设计使用 ISO1044、但我们不知道如何连接 PIN2 (输入)
问题1:什么应用于 PIN2?
Q2:PIN2是否可以置于悬空状态?

谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.