This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ISO6763-Q1:VCC1和 VCC2是否必须相等?

Guru**** 2966500 points

Other Parts Discussed in Thread: ISO6763-Q1

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1273838/iso6763-q1-do-vcc1-and-vcc2-have-to-be-equal

器件型号:ISO6763-Q1

或者它们是否可能有所不同、例如一侧为1.8V、另一侧为5V? 我们希望最大限度地减少其中一端的电流消耗、电压下降似乎就是这样。

如果电压为1.8V、是否更容易发生 EMI?