请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TXB0108 大家好,
如果信号路径是从端口(1.2V)到B端口(3.3V)。 如果端口的信号更改为High Z,该怎么办? 在这种情况下,输出B端口的状态是什么?
谢谢
Lilian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.