请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
https://e2e.ti.com/support/logic-group/logic/f/logic-forum/646105/lsf0108-q1-lsf0108
部件号:LSF0108-Q1主题中讨论的其他部件: LSF0108
您好,
我想知道如何计算LSF0108-Q1的功耗?
此致
Rana
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
https://e2e.ti.com/support/logic-group/logic/f/logic-forum/646105/lsf0108-q1-lsf0108
部件号:LSF0108-Q1您好,
我想知道如何计算LSF0108-Q1的功耗?
此致
Rana
您好,Rana:
LSF0108器件的功耗近似值为:
P = VBIA*IBIAS + N*I^2*RN/D
使用:
VBIAS := VrefB引脚到VrefA引脚的电压(典型0.85V)
Ibias := 200kOhm电阻器的电流(由(Vb+
n:=通道数
I:=通道电流(通常由上拉电阻产生)
Ron :=内部LSF通道电阻-估计高为50欧姆
D:=信号占空比(通道电流仅在低状态下适用)
外部电阻器的功率可以计算为P = I^2*R =V^2/R = I*V