请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TXS0108E 您好,
3.3V<->1.8V BIDIR电平转换器:
TXS0108E 要求的最大值为0.15V。
您能否建议如何支持 与具有VOLmax 0.45V的设备的连接?
此致,
Amir
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.