请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TXS0104E 主题中讨论的其他部件: TXS0108E
TXS0104数据表显示有效使用电压低至1.65V,其中TXS0108显示使用电压低至1.2V。
在1.2V的情况下使用TXS0104是否存在特定问题或只是文档中的疏忽?
我们在许多主板上具有TXS0104电平转换,工作电压为1.2V,没有任何功能故障,因此我们不希望进行任何更改。
请TI提供建议。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.