主题中讨论的其他部件:LSF0108, LSF0102
您好,
让我在下面确认一下。
根据数据表,9.2 .1.2 .1双向转换部分有以下说明
"EN输入必须连接到Vref_B"
EN引脚似乎应连接到此设备中的Vref_B。 但是,如果用户要单独控制EN功能和Vref_B,它是否可用?
如果您有将哪一个EN引脚连接到Vref_B的原因,请告诉我吗?
(例如,为了避免设备损坏。)
此致,
町田
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
让我在下面确认一下。
根据数据表,9.2 .1.2 .1双向转换部分有以下说明
"EN输入必须连接到Vref_B"
EN引脚似乎应连接到此设备中的Vref_B。 但是,如果用户要单独控制EN功能和Vref_B,它是否可用?
如果您有将哪一个EN引脚连接到Vref_B的原因,请告诉我吗?
(例如,为了避免设备损坏。)
此致,
町田
要使用此设备进行翻译,必须将EN引脚直接绑定到Vref_B引脚。 此外,在正常操作期间,必须允许此电压节点浮动--即电压由通过200kOhm电阻器的偏置电流设置,而不是由直接驱动引脚的设备设置。 以下是向此设备添加禁用功能的常用方法(此示例与LSF0102一起使用,但LSF0108功能相同,只是具有更多通道):
您可以在上面看到,当nFET打开(CONTROL = HIGH)时,EN引脚处的电压节点被强制为低电压,但当nFET关闭时,则允许其'浮动'到相应的偏压(CONTROL = LOW)。