This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,我正在使用TXS0101从5V转换 到3.3V (仅在一个方向)。
我在无负载的情况下测试了电路,并获得了以下结果:
底部信号为5V输入,上部信号为3.3V输出。 一切看起来都还可以。
然后,我使用电路板ESP-01 WiFi在针7 ( 图中为RXD)上进行了测试,并获得了以下信息:
导致此错误的原因是什么?
ESP-01和TXS0101之间未连接。
感谢你的帮助。