Other Parts Discussed in Thread: LSF0101
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LSF0101 大家好、
我想问是否可以使用 LSF0101将1V 传输到1.8V?
它说"允许在之间进行双向电压电平转换
0.95V 1.8/2.5/3.3/5V "。
在修订历史记录中、它显示"将双向电压电平转换从1.0更改为0.95"、您能告诉我原因吗?
谢谢你。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.